2025-04-02 3:58 AM - last edited on 2025-04-02 7:04 AM by Andrew Neil
Hi All,
I am beginner to drones. We assembled one drone using STEVAL FCU. 002. board , recommended set. of motors and. propellers along with battery.
We Chose different. frame. than. one recommended . It is smaller in size.
While flying , vertical take. off. could. not be achieved.
Can someone guide please ?
Motor connections , Clock wise. , anti clock wise in reference. to alignment. of. the boards are checked. already.
It is ST board. so. come equipped with all driver , frimware etc.
Thanks in advance.
Early and accurate response is. appreciated.
Regards,
2025-04-02 4:02 AM
2025-04-02 5:34 AM
Welcome @mmdave1, to the community!
You can't see much on your video (start of the motors at 0:2.366 > 0:2.399), but it looks like the propellers are not mounted correctly.
Regards
/Peter
2025-04-02 6:18 AM
@mmdave1 wrote:While flying , vertical take. off. could. not be achieved.
This doesn't make sense: you have to take off before you can be flying!
Do you mean that you didn't achieve enough lift with the motors?
2025-04-02 6:23 AM
STEVAL-FCU001V2 is F4, not F0.
What firmware?
The stock firmware basically used to work.
Form the video it looks like a wiring / coordinate system issue.
hth
KnarfB
2025-04-02 8:24 AM
Hi Peter,
Thanks. for prompt. revert.
We have cross checked with ST documentation and it is in line.
Sharing one photo , Motors. and propellers are aligned. in that way.
Regards,
2025-04-02 8:26 AM
Hi Andrew,
That is the issue.
It does. not. take off. properly and does not achieve the lift. though motors and everry other. parts are as recommended. by ST , except frame.
2025-04-02 8:29 AM
@ KnarfB,
Standard ST firmware STSW-FCU001 . It has come. preloaded with STEVAL FCU00V1.
2025-04-02 8:33 AM - edited 2025-04-02 8:34 AM
@mmdave1 wrote:everry other. parts are as recommended. by ST , except frame.
As beginners, perhaps it would be better to start with the actual frame, motors, and propellers provided in the kit by ST?
STEVAL-DRONE02: https://www.st.com/en/evaluation-tools/steval-drone02.html
That way you know for sure that everything is correct & compatible
BTW: What's. with. all. the. full. stops. in. your. posts?
2025-04-02 8:34 AM
The direction of rotation is correct, but which propeller with which tilt did you use where?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.