2017-10-31 12:53 AM
The FOC library is complicated and I have some difficulties to understand how to work with it. Even after reading UM1052, UM1053.
On the highest level we can start/stop a motor
if (MCI_GetSTMState(oMCI[M1]) == IDLE) { MCI_StartMotor(oMCI[M1]); } else { MCI_StopMotor(oMCI[M1]); }
But how to set velocity and current?
Another question - I have to drive DC motors as well. What should I set for this purpose?
Is there more extensive examples?
2017-12-12 10:21 AM
For the second question, did you mean brushed or brushless DC motors
PMSM FOC library is for driving the brushless ones.
2017-12-13 8:33 AM
I need to drive DC motors as well as BLDC. So I thought there is a way to set the firmware to behave like a full bridge driver.
2017-12-13 4:49 PM
I don't think FOC SDK is applicable for driving Brushed DC motors. The poles in Brushed motors are mechanically commutated vs the Brushless ones where we need complex algorithms to commutate motor windings.
If you do need an intergated solution, take a look at this document:
2017-12-14 8:04 AM
L6235 or L6229 would be perfect. But I need current 10-15 ampere.
2017-12-21 3:12 AM
Hi,
I confirm the FOC library cannot be modified to make it work as a full-bridge driver.
Moreover this driving technique is extremely complex compared to the task of driving a brushed DC motor.
I suggest you to start from an easier firmware like the
For the current ratings you need, ST can provide you a complete set of gate drivers and mosfets.
Enrico
2018-02-21 4:52 AM
I have DC motor (two wires) in my project. I have to drive it also. I have no intention to design 2 boards - one for BLDC motors and one for DC motors.
TI's library (Control Suite) deals with both types of motors.
I suggest you to start from an easier firmware like the
/external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fcontent%2Fst_com%2Fen%2Fproducts%2Fembedded-software%2Fmcus-embedded-software%2Fstm32-embedded-software%2Fstm32cube-expansion-packages%2Fx-cube-spn4.html
I don't want to use STM32Cube in my project. I'v perfectly well with SPL.
2021-06-15 1:45 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards