2023-07-21 9:05 PM
I am running the motor control workbench B-G431B-ESC1 board. The systick fires at every 2K frequency as per the user manual and the waveform matches when i toggle, but the problem is sometimes it misses as shown
I want to debug and find out why it misses those timings in between. Please suggest how do i find out? I am also running CAN in parallel at 500KBPS.
Solved! Go to Solution.
2023-09-24 10:18 AM
I modified the algorithm of CAN and behavior is ok now, i mean i transmit 3 messages at one time, after 1 sec another 3 messages with total of 12 messages
1st sec -> 3messages
2nd sec -> 3 messages
3rd sec -> 3 messages
4th sec -> 3 messages
repeat like this.
2023-07-21 10:55 PM - edited 2023-07-21 11:15 PM
What is the effect of disabling CAN?
2023-07-24 4:45 AM
Sorry for late response yes it is because of CAN task, how do i solve the problem? I will try to reduce the code in CAN ISR and put it in while(1).
2023-07-24 10:45 AM
No problem. Have you considered generating your waveform directly with a TIMER routed to GPIO or if the waveform is a bit more complex use DMA to drive GPIO and use a timer to drive the DMA timing? That way CAN ISR will not interfere with waveform generation. If needed I can provide an example code.
2023-07-24 11:42 AM
DIsclaimer: I know nothing about the motor workbench code and run-time environment.
That said, if your "systick" is the normal ARM/STM32 systick timer, it typically defaults to the lowest interrupt priority. You can change that and make it a higher priority (lower numeric value) than then CAN interrupts. Presuming of course that the CAN interrupts can tolerate some delay when the systick interrupts them. Or use a different timer (with a higher interrupt priority than the CAN interrupt) for that purpose.
Is the waveform you showed just "toggle a pin" inside the systick ISR to show when it is missed (or delayed), changing the priority may be all that is needed. If that is indeed a waveform needed by your system, then changing to DMA/GPIO instead of code in an ISR as @Johi suggested might be needed.
2023-07-24 9:28 PM - edited 2023-07-24 9:29 PM
My main concern is SysTick_Handler is missing timing in between. The code is as below.
2023-07-24 10:02 PM
Search your files for "HAL_NVIC_SetPriority(SysTick_IRQn;" (might be in STM32xxx_hal.c)
and set it to:
HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);
As BobS said: lower number, higher priority. So give some higher numbers to the other interrupts.
Check the description before the declaration of HAL_NVIC_SetPriority.
2023-07-24 10:35 PM
When i searched this is what i found
HAL_NVIC_SetPriority(SysTick_IRQn, uwTickPrio, 0U);
#define __NVIC_PRIO_BITS 4U /*!< STM32G4XX uses 4 Bits for the Priority Levels */
uint32_t uwTickPrio = (1UL << __NVIC_PRIO_BITS); /* Invalid PRIO */
hence uwTickPrio is 16, but as per the ST documentation
@PAram PreemptPriority: The pre-emption priority for the IRQn channel.
* This parameter can be a value between 0 and 15
* A lower priority value indicates a higher priority
The priority can be between 0 to 15 only.
2023-07-24 10:51 PM
Simply set both priorities to 0.
2023-07-24 11:41 PM
Ok i will update the code.