2025-01-10 7:12 AM - edited 2025-01-10 7:13 AM
MCSDK 6.3.1, FOC with STOPLL, EVSPIN32G4, this motor.
We're using a custom board based on EVSPIN32G4 as a drone ESC in a traditional sensorless configuration. Naturally, in our application the motor starts up to a low RPM under idle load and then after FOC takes over it spins up and down within the whole range as commanded by the autopilot. The MCSDK is in the speed control mode.
We have found an interesting fault condition (also recreatable with the original EVSPIN32G4): if the motor is held in place somewhat elastically, e. g. by hand, during startup, the following things might happen:
Naturally (4) produces a disaster because not only there's no fault, but even the RPM follows the setpoint, so there is no way to detect that but to look at the current, which is not a reliable indicator because it's only apparent at higher RPM.
Feels like the observer converges onto some sort of a false equvilibrium in which the stator field is rotating without affecting the motor at all. I guess this might be unavoidable without external sensors but it's a bit too easy to induce in our case.
Everything runs fine and as expected otherwise.
Perhaps this is a known condition and there're known strategies to deal with it?
2025-01-16 9:13 AM
Hello @grisharevzin,
Did you try by tuning the "Estimated limits for the speed band tolerance" levels (Speed Sensing Config.>Start-up exit condition) or the "Observer + PLL (Sensorless)" parameters (Speed Sensing Config.)?
Refer to User Manual documentation available through "Workbench tool">About>Documentations>Documentation>"User manual" tab>, "Firmware errors" link, chapter 3. and 7. for more detail.