User Activity

MCSDK 6.3.1, FOC with STOPLL, EVSPIN32G4, this motor.We're using a custom board based on EVSPIN32G4 as a drone ESC in a traditional sensorless configuration. Naturally, in our application the motor starts up to a low RPM under idle load and then afte...
Hello everyone,I have a motor control project that I'm testing out using Motor Pilot. If I generate it with FreeRTOS support, Motor Pilot can't connect to the board (the board sends a probably malformed ASPEP_RESP and then it's always a timeout).I ha...
Hi.I'm driving a PMSM with FOC (Workbench file attached for reference) with MCSDK 6.3.0 in torque mode.Main parameters:1400 Hz electrical frequency max -- therefore 16 kHz PWM100 Hz mechanical frequency max~0.03 mH line-to-line inductance~9 V/Hz Kv 0...
Hi everyone!I'm evaluating STSPIN32G4 for driving a small 6 kRPM 28-pole PMSM (up to about 30A load current - it's driving a propeller, 0.06 mH inductance, about 160 kV). Generally the performance is quite good, but I have noticed frequent STOPLL fau...
Kudos given to