2021-03-10 9:36 AM
I'm looking to use the STM32F767 as part of a motor driver. However, it is not available under the MCU list in the tool. Why is that so? Is there a way to use the tool with that MCU?
2021-05-25 1:14 AM
Dear @csotiriou
Welcome to the STM32 Community
Could you give more details to the STM32 Community about your setup -the material you use- ?
(HW and SW, CPU(s), tools and versions, board(s), motor(s) and so on)
And more especially did you use STM MC tools (such as MC_suite, MC-Motor Profile, MC-SDK, MC-workbench, and so on)?
Best regards
Laurent Ca...