cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX version problem with Motor Control WorkBench

ENGIN TANRIKULU
Associate III

hi,

When I want to generate the code, it says that the STM32CubeMX version is not supported.

ENGINTANRIKULU_0-1705580255694.png

 

Even though I downloaded the latest version, it still gives the same problem.

ENGINTANRIKULU_1-1705580255804.png

 

ENGINTANRIKULU_2-1705580255703.png

 

How can I solve this problem?

Thank you

1 ACCEPTED SOLUTION

Accepted Solutions

Hi @ENGIN TANRIKULU ,

Please provide more information about your installation to help us to replicate the issue:

* CubeMx versions installed

* CubeMx installed for "user" or for "all users" (system installation)

* CubeMx installation folder was manually moved?

* OS used and version

* OS Language

Regards

Claudio

 

View solution in original post

6 REPLIES 6
Gael A
ST Employee

Hello ENGIN TANRIKULU,

It looks like it is your MCSDK version that is outdated. You can either download the MCSDK latest version MCSDK v6.1.2 (recommended solution) or downgrade your CubeMX version to one that is supported by the MCSDK you are currently using. Unfortunately, as I don't know which version of the MCSDK software your are using, I can't give you any more precise information.

If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.

Hope this will help,
Gaël A.
cedric H
ST Employee

Hello @ENGIN TANRIKULU ,

I highly encourage you to switch to the latest MCSDK 6.2.1 version.

If you are forced to stay on a 5.4 version, the supported version of cubeMX at the release date was STM32CubeMx 6.4.0.

Regards

Cedric

 

ENGINTANRIKULU_0-1705585500619.png

I'm still having the same problem.

ENGINTANRIKULU_1-1705585548847.png

 

@cedric H @Gael A The problem is still not fixed. can you help me

Hi @ENGIN TANRIKULU ,

Please provide more information about your installation to help us to replicate the issue:

* CubeMx versions installed

* CubeMx installed for "user" or for "all users" (system installation)

* CubeMx installation folder was manually moved?

* OS used and version

* OS Language

Regards

Claudio

 

Hi @CLD  ,
Operating System Language: Turkish
The problem took some effort, but it turned out to be caused by the operating system language.