2012-01-05 8:55 PM
2012-01-09 12:11 AM
The STM32 FOC PMSM SDK OverCurrent protection acts like an emergency stop. In particular it is performed exploiting the feature of the PWM timer that disables (putting in a predefined state) the six outputs. These signals are kept disabled until the user send another start motor command (after the faut acknowledge).
Regards Gigi2021-06-21 9:38 AM
The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards