cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-PCC009v2 SDK bug

nilsjacobs
Associate
Posted on March 21, 2012 at 16:45

Hello all,

I tried to use the USB to serial interface SDK for the STEVAL-PCC009v2 dev board to write a custom driver for the L6470 (EVAL6470 board).

The included library SPI_SDK.dll works fine, but the command: DFU_GoTODFUMode() from the DFU_SDK.dll to get the board in DFU mode gives an undocumented error: 7 and does not work.

Is there a solution for this problem?
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
nilsjacobs
Associate
Posted on July 09, 2012 at 11:58

Hello all,

Unforalltunately i got no answer on my question.

I saw that there is a new  patched version of the STEVAL-PCC009V2 firmware.

Does this address my problem?

It would be nice if there was at least a changelog with all these closed source firmware.

Greetings,Nils.

Laurent Ca...
Lead II

The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards