cancel
Showing results for 
Search instead for 
Did you mean: 

How to migrate the PMSM SDK 2.0/3.0 to STM32F4?

xinzhong
Associate
Posted on December 19, 2011 at 14:49

I used to developing a servo driver with PMSM FOC SDK 2.0 in STM32F103 MCU. And I wanna make a new control board with STM32F417ZG because of its floating point unit. Can I use the SDK2.0 in F4 directly or do something. I can't find any migration information between F1 and F4 on ST website.

And I plan to update the SDK from 2.0 to 3.0, but I can�t get the source code of PMSM SDK3.0 from Chinese distributor, so can someone send me the source code. Thanks a lot.

#condiential-web-distribution
This discussion is locked. Please start a new topic to ask your question.
14 REPLIES 14
bille.stello
Associate III
Posted on December 20, 2011 at 09:35

Hello Ding,

STM32F103 and STM32F4xx have slight difference in terms of peripherals. Working with SDK v2.0 I think it's not very user friendly to apply the right modifications on the FW.

On the other hand, we are working on the SDK v3.2, it will also support - other than F100 and F103 series -  F2xx and F4xx family (always with integer number representation for the time being).

We expect to have web distribution of this new library by February 2012; depending on business details we may also arrange for you a beta release of the same FW by the end of January/beg of February.

To get source file of the web distribution v3.0 (that is the so called confidential distribution), ask your distributor to contact ST sales offices.

Best Regards,

Billino

xinzhong
Associate
Posted on December 23, 2011 at 04:12

Hi Billino,

Thank you for your reply. I’m glad to try the new MC library when you finished. I always use Keil to develop the STM32s, so the project supported by Keil will be better. My Email:

mailto:xinzhong.ding@gmail.com

, looking forward to your new release. Thanks.

brunobruno9
Associate
Posted on March 15, 2012 at 12:00

Hello Billino,

just wondering how v3.2 is coming along...it's already mid-March - is it already available for download?

cheers

kernel
Associate
Posted on May 04, 2012 at 03:44

I am a field application engineer working at a distributor in china. For now, STM32F4 motor control and frequency converter is the most suitable application. So MC libraries is the most important factor for customer's evaluation. so we expect to this libraries can release as soon as possible. If not. STM32F4 very difficult to promote.

    Now TI's TMS320F2000 and  LM4XXX,  freescale Cortex-M4 is quickly promote.
ericc
Associate II
Posted on May 06, 2012 at 19:56

I'd like an update on the v3.2 expected date as well if you can give one.

Eric

dannym
Associate III
Posted on June 05, 2012 at 11:02

I'm also looking for this for use with the STM32F4-Discovery to run sensorless brushless FOC, I saw references to SDK 3.2 but no place to download it.  

The UM1052 PDF is available for download, that says ''STM32F103xx/STM32F100xx/STM32F2xx/STM32F4xx

PMSM single/dual FOC SDK v3.2''

And it refers to the M4 here too, and it was published in March.  But there's no link to a motor control lib v3.2.

Does the 3.2 lib exist?  Is it a ''confidential'' release?
Gigi
ST Employee
Posted on July 09, 2012 at 12:23

Take a look at [DEAD LINK /public/STe2ecommunities/mcu/Lists/motor_control/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/motor_control/STM32%20FOC%20PMSM%20SDKv3.2%20Confidential%20distribution%20available%20under%20request&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580005A810128153A7244A21980BD49736843&TopicsView=https%3a//my.st.com/public/STe2ecommunities/mcu/Lists/motor_control/AllItems.aspx&currentviews=0]this post

Gigi

dannym
Associate III
Posted on August 01, 2012 at 22:26

I contacted my local support office again today, spoke with the motor control rep, and was told the STM32 FOC PMSM SDKv3.2 ''Confidential distribution'' was not available at this time and there is currently no scheduled release date where I might be able to obtain a copy.

Is its release available upon request or not?  What would be the best way to obtain a copy?

Gigi
ST Employee
Posted on August 02, 2012 at 09:25

The STM32 FOC lib. 3.2 - Confidential distribution has been released 6th of July.

Please ask him to contact microcontroller division or the motor control headquarters in Catania.

Ciao

Gigi