2020-02-24 12:35 AM
Hello. I am using Steval - spin3204 and motor jk86bls71-03-x001. I am building a project for Keil in ST Motor control 5.4.3. But I can’t start the engine with or without Hall sensors. I tried to make various configurations of PID controllers, PWM parameters, time, etc., but nothing works. Please tell me, if someone has a working project so that I can do it by analogy. A project that is located on the ST website is compiled with errors.
Here is the project I'm working with
Solved! Go to Solution.
2020-04-03 06:22 AM
Hello DTrif.1,
Are you using the following example from the MCSDK5.4.3:
Thanks and best regards,
Claire
2020-04-03 06:22 AM
Hello DTrif.1,
Are you using the following example from the MCSDK5.4.3:
Thanks and best regards,
Claire