2022-05-18 6:09 AM
Hi All,
Got it turning. Now need a guidance on where / what file and how I can control the speed.
SDK 5.4.8.
6S_STEVAL3202_SL_VM example.
Monitor connects well.
I can start the motor.
Final ramp speed does not work. The only use - setting the direction of rotation.
Measured speed raises from 0 to 4000rpm and motor stops with Fault over "Start-up failure". Motor power indicator jumps to max and stays there.
My application is simple. I need an open loop control. 2 speeds forward, 2 speeds reverse. Stop. Preferably hardware control -3 pin. The only feedback - hardware Fault output.
Questions are:
Thanks in advance for your answers.
Regards,
Edward.
Solved! Go to Solution.
2022-05-24 7:39 AM
Hi Edward,
please try replacing the function "void SysTick_Handler(void)" in the file "stm32f0xx_mc_it.c" with the following lines of code:
void SysTick_Handler(void)
{
#ifdef MC_HAL_IS_USED
static uint8_t SystickDividerCounter = SYSTICK_DIVIDER;
/* USER CODE BEGIN SysTick_IRQn 0 */
/* USER CODE END SysTick_IRQn 0 */
if (SystickDividerCounter == SYSTICK_DIVIDER)
{
HAL_IncTick();
HAL_SYSTICK_IRQHandler();
SystickDividerCounter = 0;
}
else
{
/* Nothing to do */
}
SystickDividerCounter ++;
#endif /* MC_HAL_IS_USED */
/* Buffer is ready by the HW layer to be processed */
if (LL_DMA_IsActiveFlag_TC (DMA_RX_A, DMACH_RX_A))
{
LL_DMA_ClearFlag_TC (DMA_RX_A, DMACH_RX_A);
ASPEP_HWDataReceivedIT(&aspepOverUartA);
}
else
{
/* Nothing to do */
}
/* USER CODE BEGIN SysTick_IRQn 1 */
/* USER CODE END SysTick_IRQn 1 */
Motor_Device1.uw_tick_cnt++;
MC_RunMotorControlTasks();
/* USER CODE BEGIN SysTick_IRQn 2 */
/* USER CODE END SysTick_IRQn 2 */
}
I remind you to save the project without renaming it and generate the code by clicking the UPDATE button in the project generation window of the MCSDK .
Hope this solve your issue in the 5.Y.4 release.
Regards
Alessio
2022-05-24 9:07 PM
Hi Alessio,
After replacing the code as instructed, I'm receiving error messages from compiler:
12:02:47 **** Incremental Build of configuration Debug for project 6S_STEVAL3202_HS_VM ****
make -j8 all
arm-none-eabi-gcc "C:/ST/Projects/6S_STEVAL3202_HS_VM/Src/register_interface.c" -mcpu=cortex-m0 -std=gnu11 -g3 -DDEBUG -DARM_MATH_CM0 -DUSE_FULL_LL_DRIVER -DUSE_HAL_DRIVER -DSTM32F031x6 -c -I../../Inc -I../../Drivers/STM32F0xx_HAL_Driver/Inc -I../../Drivers/STM32F0xx_HAL_Driver/Inc/Legacy -I../../MCSDK_v5.Y.4-Full/MotorControl/MCSDK/MCLib6Step/Any/Inc -I../../MCSDK_v5.Y.4-Full/MotorControl/MCSDK/MCLib6Step/Any/Src -I../../MCSDK_v5.Y.4-Full/MotorControl/MCSDK/MCLib/Any/Inc -I../../MCSDK_v5.Y.4-Full/MotorControl/MCSDK/MCLib6Step/F0xx/Inc -I../../Drivers/CMSIS/Device/ST/STM32F0xx/Include -I../../Drivers/CMSIS/Include -I../../Drivers/CMSIS/DSP/Include -Ofast -ffunction-sections -fdata-sections -Wall -fstack-usage -MMD -MP -MF"Application/User/register_interface.d" -MT"Application/User/register_interface.o" --specs=nano.specs -mfloat-abi=soft -mthumb -o "Application/User/register_interface.o"
C:/ST/Projects/6S_STEVAL3202_HS_VM/Src/register_interface.c: In function 'RI_SetReg':
C:/ST/Projects/6S_STEVAL3202_HS_VM/Src/register_interface.c:235:13: warning: implicit declaration of function 'STO_PLL_GetObserverGains' [-Wimplicit-function-declaration]
235 | STO_PLL_GetObserverGains(stoPLLSensor[motorID], &hC1, &hC2);
| ^~~~~~~~~~~~~~~~~~~~~~~~
C:/ST/Projects/6S_STEVAL3202_HS_VM/Src/register_interface.c:235:38: error: 'stoPLLSensor' undeclared (first use in this function)
235 | STO_PLL_GetObserverGains(stoPLLSensor[motorID], &hC1, &hC2);
| ^~~~~~~~~~~~
C:/ST/Projects/6S_STEVAL3202_HS_VM/Src/register_interface.c:235:38: note: each undeclared identifier is reported only once for each function it appears in
C:/ST/Projects/6S_STEVAL3202_HS_VM/Src/register_interface.c:236:13: warning: implicit declaration of function 'STO_PLL_SetObserverGains' [-Wimplicit-function-declaration]
236 | STO_PLL_SetObserverGains(stoPLLSensor[motorID], (int16_t)regdata16, hC2);
| ^~~~~~~~~~~~~~~~~~~~~~~~
C:/ST/Projects/6S_STEVAL3202_HS_VM/Src/register_interface.c:251:13: warning: implicit declaration of function 'PID_SetKI'; did you mean 'PID_KI'? [-Wimplicit-function-declaration]
-------------------------------------------------------------------------------etc--------------------------------------------
make: *** [Application/User/subdir.mk:85: Application/User/register_interface.o] Error 1
"make -j8 all" terminated with exit code 2. Build might be incomplete.
12:02:48 Build Failed. 9 errors, 11 warnings. (took 641ms)
It may be some other mods need to be done in code?
Regards,
Edward.
2022-05-25 1:05 AM
Hi Edward,
the errors raised are related to FOC functions that should not be there in the six-step project. You are likely missing something in the generation process.
I suggest to clean the folder and recreate the project from scratch starting from loading the example from 5.Y.4 as follows:
1- in the 5.Y.4 click on the example you are interested in
2- After reading, close the readme.txt file and the warning message
3- Click on "Save As" and save the project without renaming it
4- Click on project generation icon, select the toolchain and click UPDATE
5- generation process should start with the proper library version (5.Y.4-Full)
6- Load the project in your development environment and open the file stm32f0xx_mc_it.c where you have to replace the function like in my previous post
7- build and download the project to the board (or launch the debug mode...)
8- Open the Motor Pilot, load the defaultApp_6STEP and connect with Speed 115200
Regards
Alessio
2022-05-25 6:53 AM
Hi Alessio!
Thank you!
Thanks to you I've made the biggest progress in 6 month with this board!
I was able to download HAL (not LL) and it connects to Monitor!
Thanks again!
I'll be continuing my endeavors in the code to find how to control the board from code.
Thanks again!
Regards,
Edward.
2022-05-25 7:33 AM
Hi Alessio,
The errors starting to pop up when I select Sensorless + PLL or other Sensorless in Speed sensing:
C:/ST/Projects/6S_STEVAL3202_SL_VM/Src/mc_config.c:47:43: warning: initialization of 'short unsigned int' from 'void *' makes integer from pointer without a cast [-Wint-conversion]
47 | .enPWMx[0].enPWMx_GPIO_Pin = NULL,
| ^~~~
C:/ST/Projects/6S_STEVAL3202_SL_VM/Src/mc_config.c:47:43: note: (near initialization for 'Motor_Device1.enPWMx[0].enPWMx_GPIO_Pin')
C:/ST/Projects/6S_STEVAL3202_SL_VM/Src/mc_config.c:49:43: warning: initialization of 'short unsigned int' from 'void *' makes integer from pointer without a cast [-Wint-conversion]
49 | .enPWMx[1].enPWMx_GPIO_Pin = NULL,
| ^~~~
C:/ST/Projects/6S_STEVAL3202_SL_VM/Src/mc_config.c:49:43: note: (near initialization for 'Motor_Device1.enPWMx[1].enPWMx_GPIO_Pin')
C:/ST/Projects/6S_STEVAL3202_SL_VM/Src/mc_config.c:51:43: warning: initialization of 'short unsigned int' from 'void *' makes integer from pointer without a cast [-Wint-conversion]
51 | .enPWMx[2].enPWMx_GPIO_Pin = NULL,
| ^~~~
C:/ST/Projects/6S_STEVAL3202_SL_VM/Src/mc_config.c:51:43: note: (near initialization for 'Motor_Device1.enPWMx[2].enPWMx_GPIO_Pin')
First the warning above (pops up even with hall sensors selected but can be ignored)
With Sensorless selected:
C:/ST/Projects/6S_STEVAL3202_SL_VM/Src/register_interface.c:235:13: warning: implicit declaration of function 'STO_PLL_GetObserverGains' [-Wimplicit-function-declaration]
235 | STO_PLL_GetObserverGains(stoPLLSensor[motorID], &hC1, &hC2);
| ^~~~~~~~~~~~~~~~~~~~~~~~
C:/ST/Projects/6S_STEVAL3202_SL_VM/Src/register_interface.c:235:38: error: 'stoPLLSensor' undeclared (first use in this function)
235 | STO_PLL_GetObserverGains(stoPLLSensor[motorID], &hC1, &hC2);
| ^~~~~~~~~~~~
6 step can be sensorless right?
Regards,
Edward.
2022-05-25 8:12 AM
Hi Edward,
examples cannot be customized through the MCSDK GUI. So you cannot choose sensorless and regenerate the project.
If you want to run the sensorless algorithm you need to open the corresponding example in the example projects list, repeat the above steps and customize the algorithm parameters like shown in section 4.2 of the UM2916 I attached to my previous post
2022-05-30 7:47 AM
Hi Alessio,
I am opening a new project in 5.Y.4.
It is sensorless:
When it is just open, It has Hall Sensors for the Motor and in Speed Sensing.
Am I not allowed to change it to sensorless?
Motor and Speed sensing in sensorless example should be sensorless right? Or I just need to ignore these settings?
Regards,
Edward.
2022-05-31 1:55 AM
Hi Edward,
disregard those setting. If you opened the sensorless example it will run in this way despite the configuration reported in the GUI
Alessio
2022-09-20 11:11 AM
Hi ADAVE.1,
I was able to successfully run 6 step with the Steval-Spin3202, starting with the 6 step example provided by MCSDK-Y and following the steps you provided above.
Now, I have made many attempts to develop FOC with the same board Steval-Spin3202, but couldn't succeed. For that, I tried developing the code from scratch with MCSDK-Y. All I get is the following:
Note that, when I try to change the code "void SysTick_Handler(void)" I get errors due to some variables or functions not declared. Maybe that piece of code you tell us to change only apply for 6step development and not for FOC.
Please, can you write a post with detailed steps, similar than before, but now for FOC and with the same board Steval-Spin3202?
Regards,
Joseph
2022-09-21 12:25 AM
Hi Joseph,
This board is supported by MCSDK 5.Y.4 for FOC algorithm. Therefore, if you want to generate the FOC code for STEVAL-SPIN3202, I suggest you to follow the wizard.
Select New project -> Inverter -> Steval-Spin3202
Customize the parameters in the GUI as you wish, save the project and generate the code.
Regards
Alessio