2022-09-22 1:24 AM
Hi,
I am trying to run a brushless motor at constant speed and at a ramped input (from 0 rpm to desired speed and back to 0 rpm representing a triangle wave at 0.01 Hz) to rotate an experimental rig (consisting of a small shaft clamped using 2 bearing housings) up to 15,000 rpm.
The link for the motor is as follows:
I am very new to motor control, and with hopes of quick-learning I ordered the STEVAL-SPIN3204 driver board for this purpose. I have installed the X-cube-MCSDK Y (version MC SDK 5.Y.4) control software to find an example for applying to my project, but none of the example projects there are for BLDC motors. I did find an example for Shinano LA052-080E3NL1 using the mentioned driver board, but the motor parameters only show for PMSM structures.
Link for the driver board: STEVAL-SPIN3204 - Six-step brushless motor driver evaluation board for applications based on the STSPIN32F0B BLDC controller - STMicroelectronics
SDK link: X-CUBE-MCSDK - STM32 Motor Control Software Development Kit (MCSDK) - STMicroelectronics
Please could you share some knowledge about where to go from here? If I change the parameters from this PMSM examples, would it be adequate for running the bldc motor? and lastly, is the MCU board along with a DC voltage supply enough to run the brushless motor? or will I require an esc or any other additional modules for this purpose?
Many thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.