cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-SPIN3201 "ASPEP_RESP ERROR:CMD_NOK"

michelemancini2
Associate III

0693W00000HrfGFQAZ.pngI'm working with the STEVAL-SPIN3201 board

I have compiled and uploaded example "6s_STEVAL3201_HS_VM"

I have a 70mm diameter sensored BLDC motor

When I connect through the software ST Motor Pilot V0.9.9 click in "Start" Motor and the motor turns 1/4 turn and stops .

I get a "FAULT_NOW" error message "Software Error" . In Logs

"[ERROR] - MotorControlProtocol: ASPEP_RESP ERROR:CMD_NOK"

I use ST "MCSDK 5.Y.3" version.

0693W00000HrfKkQAJ.png 

3 REPLIES 3
DCuni.1
Associate

Hi,

I have the same problem. Were you able to find a solution?

Rajeswari
Associate III

Even I got the same error. I created a new WB project and configured each module with correct parameters again. Now it works.

@michelemancini2 @Rajeswari @DCuni.1 

I think this 2.5 years old ticket is not relevant anymore.

Would you agree that we close it by accepting @Rajeswari answer as Solution?

Cedric