2022-01-14 2:51 AM
I'm working with the STEVAL-SPIN3201 board
I have compiled and uploaded example "6s_STEVAL3201_HS_VM"
I have a 70mm diameter sensored BLDC motor
When I connect through the software ST Motor Pilot V0.9.9 click in "Start" Motor and the motor turns 1/4 turn and stops .
I get a "FAULT_NOW" error message "Software Error" . In Logs
"[ERROR] - MotorControlProtocol: ASPEP_RESP ERROR:CMD_NOK"
I use ST "MCSDK 5.Y.3" version.
2022-10-07 12:34 AM
Hi,
I have the same problem. Were you able to find a solution?
2024-06-19 3:33 AM
Even I got the same error. I created a new WB project and configured each module with correct parameters again. Now it works.
2024-06-19 5:21 AM
@michelemancini2 @Rajeswari @DCuni.1
I think this 2.5 years old ticket is not relevant anymore.
Would you agree that we close it by accepting @Rajeswari answer as Solution?
Cedric