cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-ESC001v1 - Motor profiler - profiling failed

Kamil1
Associate II

Hello,

I have tried to use Motor Profiler with ESC001v1 and drone rc outrunner motor: 14n12p (7 pole pairs), 6s, 600kv

Connection via St-link and Uart was succesfull, firmware uploaded to the board ESC001v1, but motor profiling failed.

Where could be a problem? How can get more information than only "profile failed" ?

Thank you

Kamil

3 REPLIES 3
ritesh
Associate II

Getting same error with

STEVAL-IPM15B + NUCLEO-F303RE + X-NUCLEO-IHM09M1 

Have you found any solution?

Kamil1
Associate II

unfortunatelly I haven't found any solution, absolutely no answer or help from ST...

Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards