2018-12-03 12:26 AM
Hello,
I have tried to use Motor Profiler with ESC001v1 and drone rc outrunner motor: 14n12p (7 pole pairs), 6s, 600kv
Connection via St-link and Uart was succesfull, firmware uploaded to the board ESC001v1, but motor profiling failed.
Where could be a problem? How can get more information than only "profile failed" ?
Thank you
Kamil
2020-02-19 02:44 AM
Getting same error with
STEVAL-IPM15B + NUCLEO-F303RE + X-NUCLEO-IHM09M1
Have you found any solution?
2020-05-14 10:01 AM
unfortunatelly I haven't found any solution, absolutely no answer or help from ST...
2021-06-27 09:55 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards