Skip to main content
PFeit
Visitor II
December 5, 2018
Question

MotorProfiler with different board set

  • December 5, 2018
  • 2 replies
  • 571 views

Hello,

I would like to know if there's a way to use the motor profiler with a different set of board then the predefine one.

I already have the NUCLEO-F302R8 and now i want to use it with a STEVAL-IPM07F. The MotorWorkbench tools allows me to use both board but not the motorprofiler.

Is there a way to tweak the motorprofiler to support other boards set?

Thanks,

Pascal

This topic has been closed for replies.

2 replies

MRyan.7
Associate III
December 30, 2018

Hello,

The only boards supported by the profiler are the ones they allow you to choose from the program (this was emphasized in a class for the MC workbench). We have used one of the stock board combinations listed to profile a motor however. When you save that motor profile, it is accessible by the motor workbench. So you can still use that profile, it is just generated by their boards.

Mr Yan

Laurent Ca...
Senior III
June 28, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards