2018-11-05 11:04 PM
When I use the motor control workbench with KEIL uvision 5.25, I get the following error:
linking...
ESC001\ESC001.axf: error: L6047U: The size of this image (33032 bytes) exceeds the maximum allowed for this version of the linker
Finished: 0 information, 0 warning, 0 error and 1 fatal error messages.
"ESC001\ESC001.axf" - 1 Error(s), 0 Warning(s).
Target not created.
I read somewhere that there are compiler options to reduce code size - which were for AC6. Can anyone guide me towards fixing these errors for uVision.
Thanks!
2021-06-22 02:08 AM
The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards