Skip to main content
Fendo59
Associate II
September 3, 2023
Solved

STM32CubeIDE & MX integrated

  • September 3, 2023
  • 20 replies
  • 8193 views
Hi,
I have some problem with STM32CubeIDE, since when I start a new project everything works well as long as I delete the file: 
"home/STMCubeIDE/workspace_1-13.1/.metadata/.plugins/.org.eclipse.e4.workbench/workbench.xmi".
However, when I exit the project, closing STM32CubeIDE, and I reopen it, recalling integrated MX, either a blank page or the MCU only is shown. I'm not allowed to do anything.
STM32CubeMX standalone works correctly, without problems.
I tried to find some solution online, nothing works but deleting the file indicated above and restart the project 
Here's my system informations:
 
Computer HP HP 250 G5 Notebook PC
SSD 500 GiB
Memory 8.0 GiB
Processor Intel® Celeron(R) CPU N3060 @ 1.60GHz × 2
Graphics card Mesa Intel® HD Graphics 400 (BSW)
O.S. Ubuntu 22.04.1 LTS 6.2.0-31-generic #31~22.04.1-Ubuntu
GNOME version 42.9
Graphics system Wayland
 
Java version:
openjdk version "17.0.8.1" 2023-08-24
OpenJDK Runtime Environment (build 17.0.8.1+1-Ubuntu-0ubuntu122.04)
OpenJDK 64-Bit Server VM (build 17.0.8.1+1-Ubuntu-0ubuntu122.04, mixed mode, sharing)
 
STM32CubeMX version 6.9.1
STM32CubeIDE version 1.13.1
 
STM32CubeProgrammer API v2.14.0 | Linux-64Bits
 
STM32 Trusted Package Creator v2.14.0 STMicroelectronics
 
Thanks for any suggestion.
This topic has been closed for replies.
Best answer by Fendo59

I will continue my work with release 1.12.1 while waiting for the solution to the problem of release 1.13.1.
Thanks for your help.

20 replies

Issamos
Super User
September 3, 2023

Hello @Fendo59 

I suggest you to Completely uninstall STM32CubeIDE and delete any remaining configuration files/folders before reinstalling (this post explain this operation). This will clean out any corrupted settings. Than reinstall it.

Best regards.

II

Fendo59
Fendo59Author
Associate II
September 3, 2023

Thanks for the reply.
I've already uninstalled with a purge and manually deleted the rest, reinstalled three times without success.
Now I try to uninstall ALL STM32 packages.
I hope for better luck.

Thank you

Issamos
Super User
September 3, 2023

Uninstall all the STM32 SW and packages and than reinstall them well be a good idea I guess.

Best regards.

II

Fendo59
Fendo59Author
Associate II
September 3, 2023

After the 8th uninstall and install (see image)

Issamos
Super User
September 3, 2023

Hope that works fine.

Best regards.

II

Fendo59
Fendo59Author
Associate II
September 4, 2023

Don't work again.

I installed version 1.10.1 and it works fine. I want to try with 1.12.1

Issamos
Super User
September 4, 2023

Hope this works for you ☺️

Fendo59
Fendo59Author
Associate II
September 4, 2023

Realese 1.12.1 works fine, 1.13.1 still doesn't work.
Can multiple releases coexist on the same computer?

Issamos
Super User
September 4, 2023

Yes, you can have multiple release in the same computer

Best regards.

II

Fendo59
Fendo59Author
Associate II
September 4, 2023

Thank you very much. 

Now I have 1.10.1 and 1.12.1, they work fine. 1.13.1 does't work :face_with_steam_from_nose:

If you want I can post the logs of 1.13.1

Issamos
Super User
September 4, 2023

Ok thanks.

Best regards

II

Fendo59
Fendo59AuthorBest answer
Associate II
September 4, 2023

I will continue my work with release 1.12.1 while waiting for the solution to the problem of release 1.13.1.
Thanks for your help.

Fendo59
Fendo59Author
Associate II
September 7, 2023

Hello,
attached here are the two log files
Thanks