STEVAL-CTM012V1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2025-01-28 01:57 AM
I have STEVAL-CTM012V1 evaluation board for 250 W. I have followed all the procedure which are mention in the manual where I first load the firmware file stsw-ctm11 in motor control work bench then click on generate code then goes into cubemx then generate code and goes into STM32CubeIDE and project is created. So my question is that the generated project is enough to run motor means we just need to upload the code into the board and it will start motor right?
Labels:
- Labels:
-
Bug-report
-
MC Firmware
-
STM32 Motor Control
0 REPLIES 0
![](/skins/images/9117C6B72C9F598A212AA17633C1CC28/responsive_peak/images/icon_anonymous_message.png)