2022-05-13 08:33 AM - last edited on 2024-09-11 04:08 AM by Andrew Neil
Hi, I am planning to buy STEVAL-CTM012V1. but when i open motor profiler this board is not available.
Pl guide how with to use this board with motor profiler software
2024-09-11 04:03 AM
I purchased STEVAL-CTM012V1 board, I also facing same issue.
2024-09-11 04:35 AM
Hello sadiq, NPI,
First of all, I'd like to apologize for the delay in replying to the original post.
I'm afraid the STEVAL-CTM012V1 inverter board is currently not supported by the MCSDK 6.3.0, and though it will soon be added to our assets, I have to warn you that profiling a motor will not be possible at all on this board for two reasons :
- It runs on STM32F0, which is not supported by the Profiler
- Available current sensing is only available with 1 Shunt, which is also not supported by the Profiler (3 Shunts only)
The only solution I can provide right now, is to create the board description of the STEVAL-CTM012V1 inverter using our Board Designer, to make it available on MCSDK at first.
Your profiling will have to be done on a different setup, and once your motor is profiled you can save it and then create a project with the STEVAL-CTM012V1 and that new motor.
If you don't want to get a new setup, I guess you could manually get the info you need for your motor as described in the MC Wiki.