cancel
Showing results for 
Search instead for 
Did you mean: 

ST Motor profiler with NUCLEO-F401

JEsca.1
Associate II

Dear

I am looking to test Nucleo-F401 with Motor driver IHM07-M1 but when stating motor profiler, this nucleo board does not appears in the list of supported board. When reading release not of Motor profiler, F401 should be in the supported board.

Please help

Thanks

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Cristiana SCARAMEL
ST Employee

You are right the Nucleo-F401RE is not available in the Motor profiler.

Anyway if you have the motor datasheet you can start a new project with ST MC Workbench software tool and upload the motor data directly inside.

If you feel a post has answered your question, please click "Accept as Solution"
JEsca.1
Associate II

Dear Cristiana, thanks for answer however my motor datasheet is not complete and profiler would be a good way to tune. I ordered F303 Nucleo to check only motor parameters. Thanks for your help.

Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards