2025-07-30 8:15 AM
Hello Everybody,
I have a high-power BLDC motor with a rated power of 200W and a nominal voltage of 24V, resulting in a current draw of approximately 10A. I intend to use Motor Profiler to detect detailed motor parameters (e.g., B-EMF constant). Could you advise on which ST control board is suitable? I know there are many control boards like NUCLEO-G431RB. Given the high current, is the control board with the Three-Shunt current sensing inappropriate? If so, what alternative control board should I select? Thank you!
2025-08-07 5:20 AM
Hello @DF_MC,
Opening BOARD in the MCSDK workbench and selecting Power Boards and Inverter Boards, you will be able to make your selection based on electrical characteristics.
The NUCLEO-G431RB is a versatile board that can meet your requirements.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.