cancel
Showing results for 
Search instead for 
Did you mean: 

ST Motor Pilot connect using Segger J-Link VCOM

Joel4
Associate II

Hello,

I have a Segger J-Link to program the eval board EVLDRIVE101-HPD.

I want to connect to ST Motor Pilot V1.2.9, but the software only looks for STLINK VCP.

Is it possible to connect to the VCOM of the J-Link?

Thanks

 

1 ACCEPTED SOLUTION

Accepted Solutions
LHOUE
ST Employee

Hello @Joel4 you can used any uart converter. Motor Pilot will use the port COM accessible through windows OS.

BRs

If you agree with my answer, please accept it by clicking on 'Accept as solution'.

View solution in original post

2 REPLIES 2
LHOUE
ST Employee

Hello @Joel4 you can used any uart converter. Motor Pilot will use the port COM accessible through windows OS.

BRs

If you agree with my answer, please accept it by clicking on 'Accept as solution'.
Joel4
Associate II

 

The problem was detected using the defaultApp.qml with the Discover Board button.

It is working now when using another GUI.

Thanks