2024-09-18 5:38 PM
Hello,
I have a Segger J-Link to program the eval board EVLDRIVE101-HPD.
I want to connect to ST Motor Pilot V1.2.9, but the software only looks for STLINK VCP.
Is it possible to connect to the VCOM of the J-Link?
Thanks
Solved! Go to Solution.
2024-09-19 12:39 AM
Hello @Joel4 you can used any uart converter. Motor Pilot will use the port COM accessible through windows OS.
BRs
2024-09-19 12:39 AM
Hello @Joel4 you can used any uart converter. Motor Pilot will use the port COM accessible through windows OS.
BRs
2024-09-20 4:48 PM
The problem was detected using the defaultApp.qml with the Discover Board button.
It is working now when using another GUI.
Thanks