2024-06-20 9:04 AM
I'm working on a project with the EVALSTDRIVE101, and my motor has Hall sensors. I'm able to use the Hall sensors with SDK 6.2, but with SDK 6.3, the processor runs to the HardFault_Handler routine if the Hall sensors are enabled (as an auxiliary speed sensor).
If the Hall sensor is enabled, the HT_Init function is called in the FOC_Init function in the mc_tasks_foc.c file. However, if I step into the function, a file opens indicating "Can't find a source file ... mp_hall_tuning.c." If I keep stepping through the disassembly, I eventually get to the fault routine. Something obviously broke in the new implementation.
Can someone tell me where the mp_hall_tuning.c file is and why I don't have access to it? Is it included in a precompiled statically compiled library or something?
Solved! Go to Solution.
2024-06-20 10:14 AM
Thank you. Initializing the pMCIList pointer solved the problem.
Could you please still tell me where the missing mp_hall_tuning.c file is? Is it included in a precompiled statically compiled library?
2024-06-20 9:46 AM
2024-06-20 10:14 AM
Thank you. Initializing the pMCIList pointer solved the problem.
Could you please still tell me where the missing mp_hall_tuning.c file is? Is it included in a precompiled statically compiled library?
2024-06-20 11:35 PM
Hello @CharlvdM ,
You are right, it is part of compiled library.