2021-01-08 4:33 PM
Often I find that MCSDK does not have the exact MCU I need to use so I need to end up modifying the CubeMx *.ico file generated from MCSDK.
In trying to determine the relationship of these files I took an existing working project and renamed the *.stmx file to *.stmx_____. I then loaded the *.ico file with CubeMx with no complaints. Next I deleted the drive_parameters.h file then had CubeMx generate new code. The result was a new drive_parameters.h file was generated.
Where does the information for this new drive_parameters.h file come from? There was no old drive_parmeters.h file and the *.stmx file was not present.
I ask this because sometimes when rebuilding my project I find all my drive_parameters.h values have changed and I need to copy the file over from an archived project.
Thanks for any insight you can give on this. A secret decoder ring would be appreciated from ST ;)
Brian
Solved! Go to Solution.
2021-01-11 7:53 AM
Hello Brian,
Once the CubeMX file .ioc is generated, it has in the middleware section a part called MotorControl, which contains all the information about the FOC algorithm, among which the "previous" drive_parameters.h file.
Modifying the CubeMX file can lead to some error, so I suggest to always generate the project starting from the Workbench (.stmcx file) .
Further modifications can be added directly to the code in the dedicated parts indicated between comments:
/* USER CODE BEGIN ... */
/* USER CODE END... */
Code inside these comments is kept when the project is generated again and not overwritten by the new code generation.
I hope this can help you in your project.
2021-01-11 7:53 AM
Hello Brian,
Once the CubeMX file .ioc is generated, it has in the middleware section a part called MotorControl, which contains all the information about the FOC algorithm, among which the "previous" drive_parameters.h file.
Modifying the CubeMX file can lead to some error, so I suggest to always generate the project starting from the Workbench (.stmcx file) .
Further modifications can be added directly to the code in the dedicated parts indicated between comments:
/* USER CODE BEGIN ... */
/* USER CODE END... */
Code inside these comments is kept when the project is generated again and not overwritten by the new code generation.
I hope this can help you in your project.
2021-06-01 1:45 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 SDK).
Best regards
Laurent Ca...