cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with dspin

sburr
Associate II
Posted on October 06, 2014 at 18:57

I have a computer with 64-bit windows 7 installed, when I start the dspin software it has an error message: unable to load spi_sdk.dll The application has failed to start because the side-by-side configuration are incorrect, it has 4.0 .net installed also.

3 REPLIES 3
sburr
Associate II
Posted on October 16, 2014 at 19:46

This forum is where messages go to die

Gigi
ST Employee
Posted on October 17, 2014 at 08:55

Ciao

Mybe you can have better luck there:

https://my.st.com/public/STe2ecommunities/motordriver_ics/Lists/Motor%20Driver%20ICs%20and%20Boards

There are covered dSpin products

Ciao

Gigi

Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards