2014-10-06 9:57 AM
I have a computer with 64-bit windows 7 installed, when I start the dspin software it has an error message: unable to load spi_sdk.dll The application has failed to start because the side-by-side configuration are incorrect, it has 4.0 .net installed also.
2014-10-16 10:46 AM
This forum is where messages go to die
2014-10-16 11:55 PM
Ciao
Mybe you can have better luck there:https://my.st.com/public/STe2ecommunities/motordriver_ics/Lists/Motor%20Driver%20ICs%20and%20Boards
There are covered dSpin products Ciao Gigi2021-06-17 1:30 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards