cancel
Showing results for 
Search instead for 
Did you mean: 

Overload Derating

JDesi.1
Associate II

I want to know the overload based derating, there will be continuous current and the peak current. If the current exceeds continuous current for a certain duration i consider overload. What to be done i do not know. Does ST has any application notes?

1 REPLY 1
Laurent Ca...
Lead II

Dear @JDesi.1​ 

Welcome to the STM32 Community

Could you give more details to the STM32 Community about your setup -the material you use- ?

(HW and also SW: CPU(s), tools and versions, board(s), motor(s) and so on)

And more especially did you use STM32 MC tools (such as MC_suite, STM32 MC Motor Profile, STM32 MC SDK, STM32 MC Workbench, the used example, the origin of the base of your application source code, and so on)?

And eventually more details about your application...

Best regards