cancel
Showing results for 
Search instead for 
Did you mean: 

NUCLEO-F302R8 not found in MC workbench?

SSeve.2
Associate

I have a NUCLEO-F302R8 that I am trying to configure via the Workbench, but there are only 5 control boards shown in the new project setup screen:

  • NUCLEO-G071RB
  • NUCLEO-G431RB
  • NUCLEO-G474RE
  • STM32G081B-EVAL
  • STM32G474E-EVAL

Thats not a lot of options, so what am I missing to get support for all the other micros?

1 ACCEPTED SOLUTION

Accepted Solutions
cedric H
ST Employee

Hello @SSeve.2​ ,

The MCSDK 6.0.0 is limited to a few boards. It is the reason why the MCSDK 5.Y is still available for download. We plan to release a 6.1.0 which will support all the 5.Y boards, and even more.

Regards

Cedric

View solution in original post

2 REPLIES 2
cedric H
ST Employee

Hello @SSeve.2​ ,

The MCSDK 6.0.0 is limited to a few boards. It is the reason why the MCSDK 5.Y is still available for download. We plan to release a 6.1.0 which will support all the 5.Y boards, and even more.

Regards

Cedric

jartim
Associate III

Any further news on when this might be? I too have the same issue - using MCSDK 5.Y is fine, but that means a whole new load of installs and additional (and possibly outdated) firmware and drivers etc.