2022-09-13 05:06 AM
What can cause currents noise in inverter board B-G431B-ESC1?
The measured currents are shown in the attachment.
2022-10-06 03:22 AM
Ciao
Seems that the peak value of the current is to small respect the full scale.
Try with current 10 or 20 times bigger the signal/noise ratio should be improved.
If you can provide bigger currents to the load then is necessary to adapt the current sensing network maybe increasing the shunt resistors.
Ciao
Gigi