cancel
Showing results for 
Search instead for 
Did you mean: 

Motor Profiler with STM32303E-EVAL + STEVAL-IPM15B 3Sh

ALiu.12
Associate II

Hi Expert, 

I wan to use STM32303E-EVAL + STEVAL-IPM15B 3Sh to run the motor profiler 5.4.8.

But the error message is shown below.

I connect the control board to PC via USB, the LD8 is red. The device manager of PC cannot see com port. 

I think the STM32303E-EVAL not provide a virtual com port, right?

How could I solve this problem?

Thanks.

Snipaste_2023-07-18_16-19-50.png

 

2 REPLIES 2
Gael A
ST Employee

Hello ALiu.12,

The STM32303-EVAL should provide a COM port, so I think the USB port you are using is not the right one.
There are two USB ports on the STM32303-EVAL, one called USB and the other one called ST-LINK. Please make sure you are using the ST-LINK one, otherwise your device will not be recognized by your computer.

Hope this will help,
Gaël A.

If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.

Hope this will help,
Gaël A.

Hi Gael A, 

I checked the connection of the control board, I sure that I connecto to the rigtt port, the device manager could see the STM32 STLINK, but w/o comport. 

I also installed the driver called "en.stsw-link009.zip"

Does it need extra driver?

Or should I connect the real COM port on the lef side of EVAL to PC ?

S__61038598.jpg