cancel
Showing results for 
Search instead for 
Did you mean: 

Motor Profiler with STEVAL-IPM30B power board

DJusz.1
Associate II

Hello,

I wanted to make auto-tune for my engine but there is no STEVAL-IPM30B power board in Motor Profiler tool. Only IPM-05, 10, and 15 are supported. Can I select IPM-15B board and run Motor Profiler with a physically connected IPM-30B?

1 REPLY 1
GMA
ST Employee

Dear DJusz.1,

Firstly, we would like to sincerely apologize for the delay in replying to your post.
If your point is still pertinent, the motor profiling result with a different power board could not be accurate as Rshunt values are different between IPM-15B and IPM-30B power boards.

 

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA