cancel
Showing results for 
Search instead for 
Did you mean: 

Motor Profiler stuck at 28%

DMeie.2
Senior II

[VERSION]: 6.2.1
[TOOL]: Motor Profiler in Motor Pilot V1.2.5
[DETAILS]:Motor Profiler gets stuck while profiling at "Profiling % 28".
Hardware used is the inverter-board B-G431B-ESC1.
[EXPECTED BEHAVIOR]: I expect the motor profiler to either finish the process or abort with an error so that I can fix any existing issues.
[HOW TO REPRODUCE]: Motor is soldered to the inverter-board, power supply connected and set up to deliver the correct voltage and enough current (12V, 30A). Motor Profiler is started and connects successfully. The required motor parameters are entered accordingly. The profiling is started. At 7%, the motor twitches once, and at 21% the motor hums for half a second. Maximum observed current is around 2.5A until then. Then the process gets stuck at 28% until the notification pops up that the measurement takes too long. The board pulls standby current.

12 REPLIES 12

How would I go about doing that?

Hello DMeie.2,

Well, I explained it a bit in my previous answer, but you can get help from the Open Loop documentation in the User Manual.

If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.

Hope this will help,
Gaël A.
DMeie.2
Senior II

I already have set a known working Start-up profile for the motor into the Profiler project.

As for Open-Loop mode, I have used this before.
However, I am not sure how to enter these values into the Profiler project, as it is not possible to have Profiler and Open-Loop mode at the same time.