2020-11-02 11:43 PM
I have IMP20B with Nucleo Board F302R8.
I tried with Motor Profiler. In over current small dot shows red and profile failed.
With same configurations i tried once & motor runs a bit.
2020-11-03 12:13 AM
Dear @Community member
To respect the forum rules for the "STM32 Motor Control" tag, I moved your entire title to the description part of the text, and shortened your title.
Best regards
Laurent Ca...
2020-11-03 12:23 AM
Dear @Community member
Sorry but I do not understand very well your sentence "In over current small dot shows red and profile failed."
Best regards
Laurent Ca...
2020-11-03 12:26 AM
2020-11-03 12:26 AM
Hello Just Zoom the corner Faults Section, Its due to External SMPS???
2020-11-03 12:27 AM
Sorry will take care of that from now onwards
2020-11-03 12:28 AM
When i press start profile to set the profile at that time process few seconds & then goes into over current fault with small dot showing red.
2020-11-30 03:47 AM
Hi Darshan,
I'm here following the link in this previous post.
I see from the screenshot the board selected in the profiler is IPM15B.
However you mentioned that you have a IPM20B. Do you confirm ?
If so, consider that the two boards are different, so maybe it could be the cause of this issue.
Moreover, even without any error, using a different board bring to an incorrect profiling of the motor values.
2020-12-01 08:36 AM
Yes you are right i used IPM20B instead of IPM15B.
I agree with your feedback with using IPM15B. but motor once runs for few seconds.
I ordered IPM15 already.
2021-06-27 09:23 PM
The question has been set only to the "STM32 Motor Control" topic (the question is only about the STM32 MC SDK).
Best regards