cancel
Showing results for 
Search instead for 
Did you mean: 

Motor Profiler failure with IMP20B and Nucleo Board F302R8

Darshan Patel
Associate II

I have IMP20B with Nucleo Board F302R8.

I tried with Motor Profiler. In over current small dot shows red and profile failed.

With same configurations i tried once & motor runs a bit.

0693W000005A8KnQAK.png

9 REPLIES 9
Laurent Ca...
Lead II

Dear @Community member​ 

To respect the forum rules for the "STM32 Motor Control" tag, I moved your entire title to the description part of the text, and shortened your title.

Best regards

Laurent Ca...

Laurent Ca...
Lead II

Dear @Community member​ 

Sorry but I do not understand very well your sentence "In over current small dot shows red and profile failed."

Best regards

Laurent Ca...

0693W000005A8mIQAS.png

Darshan Patel
Associate II

Hello Just Zoom the corner Faults Section, Its due to External SMPS???

Sorry will take care of that from now onwards

When i press start profile to set the profile at that time process few seconds & then goes into over current fault with small dot showing red.

Dario CUCCHI
ST Employee

Hi Darshan,

I'm here following the link in this previous post.

I see from the screenshot the board selected in the profiler is IPM15B.

However you mentioned that you have a IPM20B. Do you confirm ?

If so, consider that the two boards are different, so maybe it could be the cause of this issue.

Moreover, even without any error, using a different board bring to an incorrect profiling of the motor values.

Yes you are right i used IPM20B instead of IPM15B.

I agree with your feedback with using IPM15B. but motor once runs for few seconds.

I ordered IPM15 already.

Laurent Ca...
Lead II

The question has been set only to the "STM32 Motor Control" topic (the question is only about the STM32 MC SDK). 

Best regards