2024-12-02 08:43 AM
I'm trying to use a RS422 transceiver set up between ST Motor Pilot and EVSPIN32G4 development board.
I'm using an FTDI USB-Serial converter and two RS422 Transceivers with /RE and DE signals.
Is it possible using the ST Motor Pilot to use these hardware flow control signals to set the transceivers in RX/TX modes as transmission occurs?