cancel
Showing results for 
Search instead for 
Did you mean: 

motor phase voltage feedback

engomid_96
Associate

 

Hi guys, I'm working on an EV motor control project, the motor type is IPMSM, and on it’s Drive, I have found that it measures the motor voltage feedbacks (middle point of inverter legs) by Op-amps (inverting Configuration) -> MCU input.

The inverter is two-level, so we have a PWM-type waveform.

The control system uses these measurements directly on its algorithm; switching got disturbed after cutting one of the op-amps inputs off. And motor stops.

My question is that what is the application of those measurements? Does anyone have a similar experience? Industrial Drives doesn’t include this section; so, I think it’s specifically for EV traction applications.

This Drive uses a single shunt current sensing method + Hall position sensor for closed loop.

The circuit schematics and output waveforms are attached.

0 REPLIES 0