2024-09-25 1:09 AM
Hello everyone,
I have a motor control project that I'm testing out using Motor Pilot. If I generate it with FreeRTOS support, Motor Pilot can't connect to the board (the board sends a probably malformed ASPEP_RESP and then it's always a timeout).
I have verified that motor control code is working correctly with test code (the motor spins as expected):
void test_task(const void *arg)
{
vTaskDelay(5000);
(void)arg;
MC_AcknowledgeFaultMotor1();
MC_ProgramSpeedRampMotor1_F(250, 1000);
MC_StartMotor1();
vTaskSuspend(NULL);
}
Noticed that void ASPEP_HWReset(ASPEP_Handle_t *pHandle) from aspep.c is always getting called.
If I untick the FreeRTOS button in the workbench and regenerate the code (keeping all other settings), then MCP works as expected.
General params:
Maybe this is known issue and there's a fix/workaround?
2024-09-25 1:58 AM
Hello @grisharevzin ,
Could you try with the latest version of MCSDK (6.3.1) which has been released?
It should fix your issue.
BRs
2024-09-25 7:53 AM
Hi @LHOUE,
I've regenerated and recompiled everything with 6.3.1, same issue (void ASPEP_HWReset(ASPEP_Handle_t *pHandle) is always getting called if I'm trying to connect with Motor Pilot).
2024-11-14 8:32 AM
Did you find a resolution to this issue? I am having the same problem
2024-11-14 11:39 AM
Nope, sorry. It's either FreeRTOS or MCP. My intuition tells me it should be easy enough to debug but I didn't go this way.
2024-11-15 6:06 AM - edited 2024-11-15 6:17 AM
Hello @grisharevzin,
Using MCSDK6.3.1, CubeMx6.12, to generate EVSPIN32G4 project, compiling it on STM32CubeIDE, I am able to connect Motor Pilot with FreeRTOS enabled using TIM6 defalut setting.
Could you please check that Baudrate setting is aligned between Workbench setting and MC Pilot?