2022-07-13 11:59 AM
After working with FUL_5.Y.2, I need some of the features offered in 5.Y.3.
I believe I clicked on the 5.5.3 version when downloading. Is 5.5.3 actually 5.Y.2? Or did I misclick? I did have trouble downloading, as my browser crashed and sent ~12 requests .
2022-07-18 01:05 AM
Hello,
Using following link
X-CUBE-MCSDK - STM32 Motor Control Software Development Kit (MCSDK) - STMicroelectronics
You are right, the version is visible as "5.5.3".
After passed the "Agreement" and "Get Software" process, I was able to download "en.X-CUBE-MCSDK_5.Y.3.zip" file.
Best regards.
GMA
2022-07-18 06:03 AM
This is unfortunately not the -FUL version of the file.
2022-07-18 06:44 AM
Hello,
The 5.Y.4 is FUL version by default, could you this one?
GMA
2022-07-18 11:27 AM
Unfortunately the 5.Y.4 version has issues when generating pwm_curr_fdbk.c and related files, while the 5.Y.3 version does not.
Regards,
DS
2022-07-20 12:54 AM
Hello,
What kind of errors do you have?
May be that upgrading CubeMx to 6.5 and STM32 FW to V1.5 could help...
Best regards.
GMA
2022-07-29 02:23 PM
What kind of errors do you have?
Pointer is null or missing on generation of pwm_curr_fdbk.c. I've tried every single combination of firmwares and CubeMXs (include both recommended and most recent) and none work. It's a problem another employee explained earlier that was apparently in the works of being fixed.
However, my problem has been solved by reverting to 5.Y.2.
2022-07-29 07:23 PM
Out of curiosity, did you abandon using features you were originally after in 5.Y.3?