cancel
Showing results for 
Search instead for 
Did you mean: 

in MCWB 5.4.3 i can't get a Connection with the EVALKIT-ROBOT-1.

ARose.1
Associate II

im very new with EVALKIT-ROBOT-1. I loaded the EVALKIT-ROBOT-1.stmx V5.4.3 File which was delivered with the Kit into the MCWB 5.4.3. Because in can’t find a Board named STEVAL-SPIN3201 i can’t use the MotorProfiler.

When i load the EVALKIT-ROBOT-1.stmx V5.4.3 into the MCWB 5.4.3. and open the Monitor i can’t Connect to the Device. I tried all Baudrates and used the Com45 who i got new, when my RS485-Adapter was connected on USB.

I tried that first with the original Firmware delivered on the EVALKIT-ROBOT-1. I generated a new *.ioc File with the settings STM32CubeMX 5.6.1 and the Toolchain ST STM32CubeIDE and selected the STM32 FW V1.11.0 Firmware-Package (Recommended). I selected the LL-Driver-Type.

I compiled the Project Error-Free and programmed the resulting EVALKIT-ROBOT-1.elf over the STMcubeProgrammer with StLink V3 to the EVALKIT. Verify was OK.

But with this firmware, there was also no Connection in MCWB-Monitor possible.

Questions: The Connetion runs over the RS485 Cable, not over the ST-Link ist hat Correct ?

Whas is going wrong?

10 REPLIES 10
Laurent Ca...
Lead II

Adding of "STM32 Motor Control" topic.

Best regards.