2023-05-04 07:35 AM
2023-05-04 10:22 AM
Welcome, @FBoua.2, to the community!
The way you control this linear motor L12 depends on your order option.
The 6V initially only stands for the operating voltage.
There are obviously the order options S, P, I and R:
If it's Option S or P, you can even use a ready-made X-NUCLEO board:
Hope that helps?
Regards
/Peter
2023-05-04 10:22 AM
Welcome, @FBoua.2, to the community!
The way you control this linear motor L12 depends on your order option.
The 6V initially only stands for the operating voltage.
There are obviously the order options S, P, I and R:
If it's Option S or P, you can even use a ready-made X-NUCLEO board:
Hope that helps?
Regards
/Peter
2023-05-05 12:18 AM
thank you so much
2023-05-05 12:20 AM
You're welcome!
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Good luck!
/Peter