Skip to main content
Associate
November 30, 2023
Solved

X-NUCLEO-OUT01A2 compatible with NUCLEO-G474RE development board

  • November 30, 2023
  • 3 replies
  • 2155 views

Any member could advice us whether we could connect the X-NUCLEO-OUT01A2 expansion board to NUCLEO-G474RE development board.

As data brief explanation is "Compatible with STM32 Nucleo development boards" but the recommendation is mentioned " The expansion board can be connected to either a NUCLEO-F401RE or a NUCLEOG431RB development board ". This make us so confused in selection the hardware.

Thanks.

 

This topic has been closed for replies.
Best answer by Pat_ST

Hello VOANHV, 

Yes, in fact, the X-NUCLEO-OUT01A2 card is compatible with the NUCLEO-G474RE card, in the same way as it is with the NUCLEO-F401RE or NUCLEO-G431RB cards, because they are in fact Arduino compatible...

In addition, for information, the both products NUCLEOG431RB and NUCLEO-G474RE are the same, only the MCU is changed.

Hope this answer to your question.

With my best regards

3 replies

ST Employee
November 30, 2023

Hello @VOANHVU 

According to UM3184, The expansion board can be connected to either a NUCLEO-F401RE or a NUCLEO-G431RB development board.

Theoretically, the NUCLEO-G474RE and X-NUCLEO-OUT01A2 both follow the Arduino Uno V3 connectivity standard (that's why it says compatible with STM32 Nucleo board), however, there might be incompatibilities with certain features. 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Pat_ST
Pat_STBest answer
ST Employee
November 30, 2023

Hello VOANHV, 

Yes, in fact, the X-NUCLEO-OUT01A2 card is compatible with the NUCLEO-G474RE card, in the same way as it is with the NUCLEO-F401RE or NUCLEO-G431RB cards, because they are in fact Arduino compatible...

In addition, for information, the both products NUCLEOG431RB and NUCLEO-G474RE are the same, only the MCU is changed.

Hope this answer to your question.

With my best regards

VOANHVUAuthor
Associate
December 4, 2023

Thank for your support!

Best regards,