2018-09-18 8:22 AM
Hello :)
I am using ST MCSDK 5.2 for a bicycle hub motor (with freewheeling) and try to tune the startup parameters.
I get decent startup by activating "rev-up to FOC switch-over"
The downside: If the motor is still moving from the last run and I try to start the motor again, I get an over current fault. Seems like rev-up and an already turning motor are not compatible?
I feel like this is where on-the -fly startup would come in handy, but when I activate it, rev-up is no longer even available. (Ideally the software would use rev-up for a stopped and on the fly for a moving motor in my opinion)
Also I am not sure if understand the whole startup procedure with the 5 possible steps correctly.
Seems like nr1 is an alignment step to get the motor to a defined position and 2 starts the movement.
How comes that this is compatible with the rev-up option? Seems like two different ways to start the motor to me.
Maybe someone has info material or his own ideas on how to tune these parameters?
Many thanks!
2021-06-27 10:27 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
2023-10-16 8:22 AM
I find it frustrating that ST staff "move" questions when they don't fit a category. I did a google search which lead me to this forum topic... but now I have to struggle to find where you put it (your community forum is not easy to use). Can you at least provide a link to where this question was moved too?
2024-04-24 3:07 AM
@Laurent Ca...Please provide a link to where this was moved. Searching in https://community.st.com/t5/stm32-mcus-motor-control/bd-p/mcu-motor-control-forum for this post brings me straight back here. There is probably nothing there that will help me but until I see it 'It's not the despair I can't stand but the hope'! Thank you.