cancel
Showing results for 
Search instead for 
Did you mean: 

How to start PMSM in open Loop FOC and Transition to closed LOOP FOC using HALL Sensor

KE.1
Associate II

Hi Team,

Please provide API and steps to transition from an Open Loop FOC to a closed Loop FOC using HALL Sensor

I am using motor control SDK 5.4.0

Thanks,

Krupashankar

4 REPLIES 4
Laurent Ca...
Lead II

Dear @KE.1​ 

I forward your question to our expert.

Just in case, it is better to have the last SDK version (which is SDK5.4.5, and very soon SDK 5.4.6)

Best regards

==

Laurent Ca...

SkyWork
Associate III

@Laurent Ca...​ 

May i know in your SDK 5.4.6 which support "open Loop FOC and Transition to closed LOOP FOC using HALL Sensor" method ?

thanks

SZENG.1
Associate II

The SDK itself doesn't support switching speed sensor online, but you can enable both the main feedback (sensorless) and the aux feedback (hall), and add a piece of code to switch the sensor properly.

CKlei.1
Associate III

I'm interested in that topic as well.

@Laurent Ca...​  Could you specify a little bit deeper how to switch between the both speed feedback modes? I couldn't find the right "spot" where this could be done.

Thank you very mutch!