User Activity

I'm using MCSDK 5.4.5 in a high torque BLDC application.DC bus voltage: 600V, motor power: 4kW, Hall sensors, current sensing with two insulated current sensors (7mOhm).I had the effect that the motor power, returned by the API, switched to a negativ...
We're using STM32 MCSDK to control a high torque BLDC motor. The motor is equiped with hall sensors. Due to high torque at startup, we start the motor in torque mode. When running, we would need the speed control mode.But if we change the control mod...
Kudos from