2020-05-06 08:18 PM
Hi,
I have a P-NUCLEO-IHM03 dev kit which comes with a iPower gimbal motor (GBM2804 – 100T) , NUCLEO-G431RB and a power shield. I am running the 'Speed Ramp with potentiometer on P-NUCLEO-IHM03 kit' example in the motor control workbench.
My intention is to run it at very low speeds, typically 5 rpm in a sensorless configuration. The example works fine for higher speeds >300rpm. There is also jerks when it starts up and the motor starts only after the pot is moved past a minimum offset value. Kindly help me in configuring the parameters in the Motor Control Workbench to achieve the same.
Thanks,
Vimal
Solved! Go to Solution.
2020-05-11 05:56 AM
Dear Vimal,
Sorry but if you want to use very low speed with the actual code, you will need a sensor...
Best regards,
Claire
2020-05-11 05:56 AM
Dear Vimal,
Sorry but if you want to use very low speed with the actual code, you will need a sensor...
Best regards,
Claire
2020-10-21 09:56 AM
Is this a limitation of the sensorless observer?
2020-10-21 10:41 AM
Dear @BTrem.1
Yes, it is. For the moment and on the midterm.
Best regards
Laurent Ca...
2021-06-21 11:03 PM
The question has been set only to the "STM32 Motor Control" topic (the question is only about the STM32 MC SDK).
Best regards