2020-09-01 9:35 PM
Original title is (before moderator's edit):
"I tried to operate STEVAl-SPIN3202 board.
But I couldn't operate.
I'd like to solve the issue one by one.
So, please support me or send the advice."
I want to operate STEVAL-SPIN3202 board by library on CubeIDE 1.4.2 with CubeMX 6.0. I.
First I made ioc fail to used Mortor Control Work Bench 5.4.4.
So, I download and load STEVAL-SPIN3202_HALL_SDK544.stmx file.
In the created ioc file, STM32 model number is STM32F031C6Tx.
But actual model number in STEVAl-SPIN 3202 board is STM32F103C8Tx.
Is it necessary to make ioc file by manual?
is It ok to used STEVAL-SPIN3202_HALL_SDK544.stmx file?
Please teach me or send the advice.
My enviromente is following.
PC : Windows 10
STM32Cube MX : Version 6.0.1
STMCube IDE : version 1.4.2
Motor Control Workbench : 5.4.4
2020-09-02 8:57 AM
Hello TNITT.2,
As I understand you have used Motor Control Workbench to create .stmcx project then you run the generated CubeMx project.
I doubt that this an STM32CubeMX problem, it is more related to ST Motor Control, so it will be more helpful to post this question under https://community.st.com/s/topic/0TO0X000000BSrWWAW/motor-control-firmware-and-software.
Regards,
Khouloud.
2020-09-02 11:21 PM
Dear Khouloud,
Hello.
Thank you for your reply and advice.
I ask my question at your indicated place.
2020-09-18 6:10 AM
Dear TNITT.2
Could you give a real title (as short as possible) at your post in order to make the forum useful for everyone and not copy a chat sentence.
Thanks by advance.
Laurent C.
2020-09-22 12:47 AM
Dear TNITT.2
I changed the tilte of this post from :
"I tried to operate STEVAl-SPIN3202 board.
But I couldn't operate.
I'd like to solve the issue one by one.
So, please support me or send the advice." (that I moved in your text message)
to:
"How to configure ioc file to operate STEVAL-SPIN3202 board with MC Workbench?"
Please do not hesitate to change it again if you need.
Thanks for your understanding.
Laurent C.
2020-10-22 12:36 AM
@TNITT.2
Hello,
Please, could indicate if you are using 6-steps or FoC algorithm ?
However, and FYI, the STEVAL-SPIN3202 board is embedding a STM32F031 MCU.
Thanks a lot,
Best Regards,
PBo
2020-10-22 2:14 AM
Hello @TNITT.2
where did STEVAL-SPIN3202_HALL_SDK544.stmx come from?
Moreover, the STEVAL-SPIN3202 is an evaluation board based on the STSPIN32F0A (system in package with STM32F031C6 MCU integrated).
Please, share with us more details on your application requirements as abovementioned by @PBo for a better support.
2020-11-02 12:51 AM
Dear @TNITT.2
As you do not answer, I guess you don't have to solve this problem anymore, therefore I consider this thread closed.
If not, feel free to reopen it by posting a new answer.
Best regards
Laurent Ca...